Part Number: SN65HVD74
Other Parts Discussed in Thread: SN65HVD30
Dear *,
1)
can you tell can we use SN65HVD74 instead of SN65HVD30 ?
2)
as the SN65HVD74 has internal integrated ESD diode, ther is no need to use additional external ESD diodes?
3)
we want to replace ISL3280EIHZ-T with SN65HVD74 and only use the RX channel of the SN65HVD74 is this ok?
also what should we do with unused pins Y,Z,D ?
Best Regards,
David.