This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P/N TLV5619CPW

Good day,

i have a question about the Date Code of the following part.

Where is the Date Code and what year would it be:

  • Hi Eray,

    The "1" in 1B would indicate that these are from either 2021, 2011, or 2001, 1991, and the "B" indicates the month, in this case that would be november.  Unless you just purchased these devices, then I would expect that these are from November, 2011.  It is impossible to tell for sure without confirming the lot trace code, but we do not offer that service on the e2e forums.  You need to reach out to your authorized TI distributor where you purchased the devices.

    Thanks,

    Paul