Part Number: TCA9800
Other Parts Discussed in Thread: SN74AUP1G17
Hi,
In the customer's barcode scanner, the RTC clock is required. The level of the clock generated by the active clock generator is relatively high (3.3V), while the MCU can only accept 0.85V. Can TCA9800 be used to connect the generator and MCU? I think TCA9800 supports a rate of 400kHz, which is sufficient for the RTC clock signal. Is it right?
Or is there a better solution or device?
Many thanks!