This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1044RNQEVM: Can I use single TVS diode instead of TPD6S300?

Part Number: TUSB1044RNQEVM
Other Parts Discussed in Thread: TUSB1044, TPD6S300, TPD1E0B04

Hello TI experts,

my customer considers TUSB1044 for their new product, and I have one question.

in TUSB1044 EVM schematic, there is one TPD6S300 for ESD protection.

but customer cannot use it because PCB is very small, they want to use single TVS diodes on each line.

is it possible to design schematic like this?

I attach the TVS diode which customer has lots of stock.

ON-SEMI_tvs_smd0201_0.17pF_usb3.x_thunderbolt3.0__ESDL2011_D-1504652.pdf

or I would appreciate if you recommend TVS diode if I can use it.

Best regards,

Chase