This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: Do we have a requirement of the DSI input overshoot/undershoot

Part Number: DS90UB941AS-Q1


Hi team,

I have an input/output question about 941/960/983:

Do we have the overshoot and undershoot of the DSI/DP input and about the CSI-2 output?

Since I have seen a peak interference amplitude about 941AS DSI input:

So from my understanding it means that if the DSI overshoot/undershoot voltage exceed the maximum 200mV, the 941AS will get interference by the unstable DSI input right? Could I understand the parameter as the "overshoot/undershoot"?

If so, what about the overshoot and undershoot  of 983 DP, 960 CSI-2 signal and what about the LVDS overshoot/undershoot requirement? Thank you.