Hi team,
My customer considers to use TRS3243EIRHBR and he is asking some questions.
- Is >10V rating of capacitor for C1-C4 enough?
Though the datasheet states that abs rating of V+/V- is ±7V, there is no description about max voltage of C1pin and C2pin. - The datasheet states that "Test conditions are C1–C4 = 0.1 μF at VCC = 3.3 V ± 0.3 V; C1 = 0.047 μF, C2–C4 = 0.33 μF at VCC = 5 V ± 0.5 V".
What if each C1-C4 has greater than these capacitance(e.g. 1uF)?
Is there any concern for rise/fall time of signal?
Of course, the customer will use recommended capacitance, but he would like to make sure if a little bit bigger capacitance is okay or not in case shortage of capacitor.
Best regards,
Shota Mago