Part Number: SN65EPT21
Hi Team,
My customer have following questions about SN65EPT21. Could you kindly help? Thanks.
1. Definition of VIH and VIL. Does it mean if D and D bar pin have input signal ranging 2075mV~2420mV, it will be seen HIGH inside IC. And if input signal ranging 1355mV~1675mV, it will be seen LOW inside IC?
2. If 1. is correct, when VCC is fixed, what will output be when D and D bar pin have input signal ranging 0~1354mV or 2421~3300mV?
3. What is VIHCMR? I couldn't understand it from datasheet.
4. What is VPP? I couldn't understand it from datasheet.
Thanks.
Regards,
Jo