Part Number: PCA9539
Hi, Team.
I'm using PCA9539 IC for controlled LEDs.
In order to operate the LED, 'H' was allocated on the P-Port.
Our VCC is 3.3V.
Then shouldn't there be 3V in the P-Port out level?
However, about 1.4 V (Vrms) is output as the square wave came out.
Is it the characteristic of Chip to came out a square wave? If not, do I have to set it up separately?
Thank you.
Best Regards.