Part Number: TUSB9261
Other Parts Discussed in Thread: CCSTUDIO
Hello TI!
I'm looking into the feasibility of replacing a Cypress FX3S chip with the TUSB9261 + a SATA2 to SDIO chip, I've had a look through the technical reference and in 8.1 of the technical reference found "A SPI flash device contains the firmware that is loaded into the TUSB9261 after the deassertion of RESET".
Does this mean the ONLY way to load firmware onto the TUSB9261 is via SPI? Is it not possible to have a dedicated partition on the SATA drive?
I'm also curious as to what level of control we have over the firmware of the TUSB9261? We want to make it a composite USB device with several different interfaces (MSC + HID + HID currently). in the future we'd like to include a CCID smart card interface as well, is this possible?
Regards!
Fujimi