Part Number: DP83848M
Other Parts Discussed in Thread: TPD4E05U06
Hello,
we're using the DP83848M in a PoE powered device. It's connected to a PoE capable transfomer like this:

The raw PoE power is then further processed by a bridge rectifier and filtering to make 5V DC (and from there on all the voltages required)

In the production we see the following failure in an alarming quantity: the Ethernet PHY does not work anymore (OS report no link). It's still visible to the host, the registers can be read and written (MDIO access). So the PHY part that talk to the MAC works fine, but there is no link established. Replacing the PHY solves the issue.
The PHY datasheet shows the following parameters:

I assume they also apply to the RX/TX pins of the PHY. We might have some PoE related transients (plug/unplug events? The scope does show spikes well above 10V) - but will they cause any harm on the secondary side?
Is my circuit between PHY and transformer sufficiently robust?
We did find a few instances where due to improper soldering the center tap of one of the two coils on the secondary side was not properly manufactured - but I'd expect that to just give no link, no to damage the PHY transceiver.
Best regards,
Lo