Part Number: TDP142
Hi
Does TDP142 support 8k 60hz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It can support 8k@60Hz with DSC.
Thanks
David
Hi David
With the DP feature, it starts to act after power-on. The transmitter and receiver communicate with each other through AUX. Before the image data is officially transmitted, The connection will transmit a series of special data patterns (Pattern), the output (Source) can send out four different signal amplitudes and four different signal characteristic levels to determine whether the connection is successful Can it be said that when testing HBR3, as long as the pre-emphasis of SW-0 400mV/SW-1 600mV/SW-2 800mV/SW-3 1200mV is tested OK , Then the SI in DP1.4 is OK
Hi,
Please also make sure the link training (send out four different signal amplitudes and four different signal characteristic levels to determine whether the connection is successful) is done at 8.1G for the SI to be considered as ok.
Thanks
David