Other Parts Discussed in Thread: XIO2001
I am implementing a XIO2001 bridge chip into my design and I have a couple general questions.
1) What are the recommended PCI resistor pull-up values for the INT#, DEVSEL#, FRAME#, etc... signals?
2) What is the VREG_PD33 signal and what difference does adding a pull-up verses a pull-down make?
3) It is recommended that a 50Ohm series resistor be use to connect CLKOUT_6 to the CLKIN pin. Is it also recommended that a 50Ohm series resistor be used on the used clocks? What about the unused clocks? Should a pull-down of some value be added to prevent the unused clock from adding noise into the circuit?
4) For confirmation, the combined power pins are not to be connected to the power rails supplying the device. Only bypass caps are to be added.
Thanks in advance!