Part Number: TUSB1044
Other Parts Discussed in Thread: TUSB211
Hello TI experts,
my customer drew 1st schematic using TUSB1044.
could you review the schematic and artwork?
and here is the question from the customer.
1. in the schematic, the folw of usb 2.0 signal is from host connector(J6) -> USB mux(U12) -> USB conditioner(U13) -> to target side connector(J1). is it right sequence? or should we change the sequence of U12 and U13?
2. how should we set DIR[1:0], FLIP and SWAP pin if the direction is fixed?
(ex. only J6 to J1 / or only J1 to J6)
3. we do not consider using of display port but we routed just in case. (AUXP(N), SBU1(2))
but if there are any bad effects to other signals like USB3, we are going to remove these routings. please check this point.
4. as the same view of no.3, we connected CTL1 and HPDIN to GND (not using display port) please also check it.
i attach the schematic and *brd artwork file for your convenience. Thanks.
Best regards,
Chase