Part Number: PCA9306
Hi,
We received PCN 20211019000.1 which affects two of the PN (PCA9306DCTR & PCA9306DCTT ) that we currently buy from TI.
We have the following questions
- Are the thermal changes a result of a process change? Are they intentionally making these changes and if so, why?
- Seems like the MIN/MAX value change was a type in the original version of the specification, but let me know if that is not the case
- Is the following stating a package change or is this part # change only? is this package used in the affected PN?