Part Number: DP83869HM
Hi,
We are using DP83869HM in RGMII to copper mode with auto-negotiation enabled. RGMII side is connected to Xilinx Zynq PS. HW straps configured to 1000Mbps. We are debugging through u-boot using mii utility.
Please refer to the PHY register values
reg 0x0-->0x1140
reg 0x1-->0x796D
reg 0x9-->0x0300
reg 0x10 --> 0x5048
reg 0x1f --> 0x0000
reg 0x1df (opcode mode register) appears to be 0xffff. On writing to the register using mii write, value appears to be same.
We tried disabling auto-negotiation, reducing the speed to 10Mbps & 100Mbps on both link partner and phy. We are still not able to ping.
Expecting your help in resolving the issue.
Regards,
Derryl
.