Other Parts Discussed in Thread: TIDA-00527, , THVD8010
I'm looking for a circuit that allows 12V power delivery solution and low-speed communication over two wires in an automotive application. The data rate on this bus can be very slow, and only needs to exchange a few simple messages.
One idea is to use UART over RS-485. I've reviewed TIDA-00527 and THVD8000, but these solution are not auto-qualified.
Would you have any other auto-qualified solutions (existing or roadmap) for this application? Thanks.