This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25833-Q1: Is it possible to bypass TPS25833-Q1's DP ?

Part Number: TPS25833-Q1


Hi Team,

There is a good new that we could DIN TI product!

Currently new project have USB POWER application, for 2.1A & 3A. 

Because the SOC selected by the customer has built-in BC1.2,

1.Is it possible to bypass DP or have a suggested connection method?

2. Or other more suitable solution?

3.Or If we could disable TPS25833-Q1's BC1.2? then we can just use SOC's BC1.2