This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1520: What's the receiver end status when △VOD reach at 50mV?

Part Number: THVD1520

Hi Team,

THVD1520 datasheet indicate △VOD's range is +/-50mV. What will happen at the receiver side if the VA and VB is approximate to 0 and △VOD exactly equal to 50mV? Thanks.
Best Regards,
Tess Chen
  • VA and VB will not be zero.

    The datasheet guarantees that the differential output voltage is at least 1.5 V, i.e., VA is at least 1.5 V above VB, or VA is at least 1.5 V below VB.

    The ΔVOD specification says that the absolute difference between these cases is at most 50 mV. In other words, if in one state, VA is 2.5 V above VB, then in the other state, VA will be somewhere between 2.45 V below VB and 2.55 V below VB.