Part Number: TUSB8042A
Hi,teams
The data sheet has the following wording:
The TUSB8042A does not have specific power sequencing requirements with respect to the core power (VDD) or I/O and
analog power (VDD33) as long as GRSTz is held in an asserted state while supplies ramp.
Does the I / O signal include XI pins?
I would like to input the signal of the external oscillator to the XI pin at the following timing.
(Inject 24MHz clock before powering on TUSB8042A)