Part Number: DS90UB960-Q1
Hi team,
My customer has encountered an issue that when they unplug the camera, the 960 could send message/detect the unplug information and transmit it to SoC while when the camera is plugging in, the 960 could not detect and could not send an information to SoC 8155. The SoC 8155 pin 16(CAM_INTB) connected to our DS90UB960Q1 pin 6, SoC 8155 is monitoring the pin 16 (cam_INTB) status. Could you please kindly help to analysis the issue? Why could not detect the camera plug in but could detect the camera un plug? Thank you.