Part Number: DS90UB964-Q1
Hi team,
Is there any Single Deserializer with 2x CSI-2 Output? Instead of using 964 or 960, this is for application such as driver monitor, that only one camera is connected but 2x CSI-2 Output is needed.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB964-Q1
Hi team,
Is there any Single Deserializer with 2x CSI-2 Output? Instead of using 964 or 960, this is for application such as driver monitor, that only one camera is connected but 2x CSI-2 Output is needed.
Hello,
Would the CSI two outputs be the same CSI data? If so, 954 has only two RX ports but the ability to split the CSI port into two 2-lane ports with one being for replication. This should be able to meet your needs.
Regards,
Nick