Part Number: DP83867IS
on the datasheet (page 5 - pin functions ) pin 33 - "SGMII COP" is declared as "driven by the PHY "
while its diff pair - pin 34 - "SGMII CON" is declared as "driven by the MAC".
both of them are noted as "outputs"
my first question is what should be the direction of the SGMII CLOCK ? I/O ?
if the answer is output - what should be the conditions (configuration ) in order to generate this clock output - (will STRAP configuration be sufficient? or must is be done via the SMI configuration ? )
regarding two additional input pins (27,28) SGMII_SIP/N - they are stated to be synchronous to the diff SGMII clock input - this stands in contradiction the definition of SGMII_COP/N which are noted as "Output" .