Part Number: DP83TC811R-Q1
If Wol is activated, there will be a signal toggling on the INH pin, and this PIN can be used to control the rest power supply on the board, is it?
Do you have any reference design for the remote wake up function?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC811R-Q1
If Wol is activated, there will be a signal toggling on the INH pin, and this PIN can be used to control the rest power supply on the board, is it?
Do you have any reference design for the remote wake up function?
WoL will not toggle INH pin. It can only toggle a configured GPIO (GPIO configured to toggle on reception of WoL packets).
If you are interested in TC-10 like remote sleep entry and exit use-cases, I will suggest you to use DP83TC812. 812 can wake up remotely and will toggle INH pin.
--
Regards,
Vikram
Hi Vikram Sharma99,
Thanks for your reply. I am sorry that i didnot catch up your meaning.
On my understanding, if DP83TC811R-Q1 is in sleep mode then the INH will be high, and if it is in other mode, the INH will be low, is it right?
If so, i can use this INH pin to control other ciruicts on my board in oder to synchronize the status of DP83TC811R-Q1. That means if DP83TC811R-Q1 in sleep mode, other circuits on my board will also be in sleep mode is controlled by INH pin through some logic device of MCU.
WoL is different from TC-10 sleep mode. For using WoL PHY will be active and not in sleep mode and hence it will not be controlling INH signal . Are you interested in sleep mode or WoL?
Hi Vikram Sharma99,
Thanks for your reply. I am sorry i am new to this area.
I am instersted in both sleep mode and WoL.
If WoL is used, PHY will be active and INH will be low, is it right?
If PHY is in sleep mode, INH will be high, is it right?
From datasheet, there is a decrption like this:
When a qualifying WoL frame is received, the DP83TC811R-Q1 WoL
logic circuit is able to generate a user defined event (either pulses or level change) through any of the GPIO pins
or a status interrupt flag to inform a connected controller that a wake event has occurred.
How can we define event through GPIO if WoL frame is received?
Hello
You may program IO_CNTRL1, IO_CNTRL2 registers to get the required indication during WoL event.
Depending upon the functionality defined in WoL_CFG, these programmed GPIOs will toggle.
--
Regards,
Vikram