Part Number: DS100BR210
I'm planning to use DS100BR210 for isolating the network interface of a PC (100 Mbps) upon receiving a digital signal. I tried the basic pin mode control (ENSMB = 1kOhm to GND) with EQ and DEM set to 0 and VOD_SEL set to 1. MODE pin was set to 1 and TX_DIS to 0. VDD_SEL was pulled to 0 for enabling internal regulator. The Tx and Rx lines were given directly without decoupling capacitors. The circuit was NOT working as expected. I tried measuring the Vdd pin which was showing 0.7 V as against expected 2.5 V. I tried removing all connections other than Vin, VDD_SEL and GND but the voltage at Vdd was still 0.7 V. s there anything that I'm doing wrong? Just for the sake of completeness, I did not connect any bypass capacitors across Vdd. But I believe that the regulator output should be available even without it.