Part Number: TIC12400-Q1
Hi experts,
I found the datasheet says that the VDD is for the SPI communications. So the device can normally working if I don't apply VDD power? Is polling mode and wake up still work without VDD?
Thanks
BR
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIC12400-Q1
Hi experts,
I found the datasheet says that the VDD is for the SPI communications. So the device can normally working if I don't apply VDD power? Is polling mode and wake up still work without VDD?
Thanks
BR
Frank
Frank,
Yes, these functions will still work without VDD, however, in order to configure polling mode, the SPI registers will need to be written. So if VDD is removed after configuration is complete, then yes this will work, otherwise VDD will have to be supplied at some point.
Regards,
Eric Hackett