This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8043: We are observing the USB 3.0 connection detected in USB 2.0

Part Number: TUSB8043


1. We are using the TUSB8043 USB HUB controller in our USB 3.0 camera products 

2.Four boards observed USB 2.0 connection instead of USB 2.0

3.And the issue was resoled after solder touch up on the pins around ,but as per X-ray reports the solder is fine .

Part Details

Part Number : TUSB8043RGCT

Part description : USB Interface IC

MFG: Texas Instrument

Date Code: 2001,1830

Invoice # : 5458294032 (DC#: 1830)

Our Schematic :