Hi
Need a solution for bridge/ethernet controller (Interface: PCIe/SATA/USB) with below specification

PCIe Gen2 x1
USB 2.0 (so can accept lower data rate limited to USB 2.0)
The intention here is to provide Gigabit ethernet connection to application processor so PHY is not required.
The bridge and application processor are on separate board so for less Board-to-Board pin count SGMII preferred.
Please suggest any product or combination of product which can be considered.