Part Number: TCA39306
Hi, I'm interested in using the TCA39306 in a series configuration. I'd like to connect a 1.8V I2C bus to a 3.3V I2C bus using a TCA39306, with multiple devices on both the 1.8V and 3.3V domains. I'd also like add a second TCA39306 to convert from 3.3V to 5.5V for another set of devices at 5.5V. Assuming capacitive loading is kept in check, is there any issue with this type of series connection of TCA39306 devices?
Thanks!