Part Number: PCF8575
HI,Staff
PCF8575データシート(SCPS121H) page13
[8.2.2 Simplified Schematic Diagram of Each P-Port Input/Output]
I have a question on this schematic.
There is a 100mA current source at the point labeled IOH.
If the upper FET is turned on, it is possible to source 100mA when the port output is VOH.
In the actual data sheet, the IOH is 30uA (min), 300uA (max).
I want to output 20mA from the port to drive the LED.
Is it possible to output this 100mA current source as a port?
Thank you for your cooperation in solving the problem.
best regards
cafain