Part Number: DS90UH948-Q1
Hi team,
I have a question about AC coupling capacitor value of FPD-LINK3 devices.
I plan to design DS90UH948 display which can be connected to either UH941 or UH947 over coaxial cable.
Recommended AC coupling value in the datasheet is
For UH947 : 0.033uF (0.015uF to GND)
For UH941 : 100nF (47nF to GND)
If I need to communicate with both serializers, how much is the recommended AC coupling capacitor at coaxial cable?
regards,