Part Number: SN751178
Hello support team,
Customer ask SN751178 VOH max value, could you support? They don't need to guarantee, but they need reference information for design.

Thanks,
Koji Ikeda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN751178
Hello support team,
Customer ask SN751178 VOH max value, could you support? They don't need to guarantee, but they need reference information for design.

Thanks,
Koji Ikeda
The purpose of a differential driver is to generate a voltage drop of at least ±1.5 V over a 54 Ω load between the two output pins. The absolute voltage does not really matter for a differential signal, so it is not guaranteed. (What does the customer need this value for?)
The common-mode voltage (see figure 1) has specified limits, but they are not useful for deriving VOH.
The output schematic shows that due to the NPN transistor, VOH is at least one diode drop (0.7 V) below VCC.