Part Number: DS90UB941AS-Q1
Hi All,
When CLK is not input to DSI (open state)
I2C connection to DES may not be correct in the route of CPU → Ser (DS90UB941) → Der.
Is the following method the best way to deal with this?
If there is no valid input in DSI, set Bit3 in the RESET CTL register to ‘1’.
If there is a valid input in DSI, set Bit3 of the RESET CTL register to ‘0’.
Best Regards,
Ishiwata