Part Number: THVD1450
Hi Experts,
The datasheet says that THVD1450 D pin supports internal pull-up.


1. Is it correct that D pin has internal pull-up?
2. With internal pull-up, is any external pull-up resister unnecessary?
3. What is the internal pull-up resister value?
Customer measures D pin and the level of D pin is around 2.5V with VCC=3.3V. No load other than probe is connected on D pin. We are assuming there is several M ohm internal resister.
Regards,
Uchikoshi