Part Number: TUSB8020B
Hello team,
- If the upstream port is connected to an internal CPU, do we need to have these signals ac coupled?
- If coupling is needed, should only TX side(CPU->USBHUB) be OK, or RX side(USBHUB->CPU) needs coupling too.
From datasheet 9.2.2 graphs, it could be read that AC coupling capacitor is needed between USB_SSTXx pins and connector.
Also, the E2E thread below was about similar case but was about downstream port.
> TUSB8020B: AC coupling of internally used downstream tx signals
Best Regards,
Ryotaro Fukui