This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E-EVM: Can't communicate through a pair of DP83TD510E-EVM as media converters.

Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO, DP83TD510E, DP83822I, DP83TC811EVM

Hi support team,

We have 2 DP83TD510E-EVM and we want to use them to evaluate the 10BASE-T1L signal (and in a later stage to use them to connect a normal ethernet device to a 10BASE-T1L switch, only for lab conditions of course).
So we just want them to work like this for the moment: ethernet device <-> DP83TD510E-EVM <-> DP83TD510E-EVM <-> ethernet device.

Is it possible to use the evaluation modules in a topology as mentioned above, without modifying the hardware or using the MDIO?
What are the jumper locations for the two boards to make this work?

In case hardware modifications are necessary, which ones?

I read the user guide multiple times but I can't find the necessary steps to realise the topology mentioned above.
The power is connected to J12, and it seems like the 10BASE-T1L link is established (I'm not sure), but the LEDs on the RJ45 connectors don't light up, the ethernet devices on the other end also have an inactive RJ45 link.

Thanks in advance and best regards.

Mathieu