Other Parts Discussed in Thread: TMDS442
I need to individually switch 3 different DVI sources to 5 different receivers. Can I cascade one of the outputs from the TMDS442 to the input of an SN75DP128, and then connect those two outputs to the inputs of two more SN75DP128?