Part Number: TUSB1002
Other Parts Discussed in Thread: TUSB522P, ,
Dear team
Does TUSB1002RGET and TUSB522PIRGER could replace each other?
Many thanks
Denny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Denny
Both are the same package but not exactly pin to pin compatible with each other. For example, pin 6 is GND in TUSB1002 while NC in TUSB522P . So you will have to take care of the pin difference in the PCB design.
The TUSB1002 also supports 10Gbps while the TUSB522P can only support up to 5Gbps.
Instead the TUSB1002, I would recommend them to use the TUSB1002A.
Thanks
David