Part Number: SN65LVDS93A
Hi,
The SYSBOOT 0 to 18 terminals of the CPU (AM437x) are connected to the D0 to 15, D24, D25, and D26 terminals.
In order to maintain the desired level during power-up, the SYSBOOT pin is connected with a 10k ohm pull-up or pull-down resistor.
Q.
Does D0-D26 of this device have an internal pull-up / down during SHTDN=Low?
Customers are concerned that the internal pull-up will prevent the BOOT sequence from being selected correctly.
Best regards,
Hiroshi