Part Number: TFP410
Hi,
The SYSBOOT 0 to 18 terminals of the CPU (AM437x) are connected to the DATA0~15, DE, HSYNC, VSYNC terminals.
In order to maintain the desired level during power-up, the SYSBOOT pin is connected with a 10k ohm pull-up or pull-down resistor.
Q.
Does DATA0~15, DE, HSYNC, VSYNC of this device have an internal pull-up / down during PD=Low?
Customers are concerned that the internal pull-up will prevent the BOOT sequence from being selected correctly.
Best regards,
Hiroshi