Part Number: TUSB321AI
Other Parts Discussed in Thread: TUSB1044, TUSB321, TUSB1044RNQEVM
Hello TI experts,
My customer considers TUSB321AI while using TUSB1044.
actually I asked about TUSB1044, and another expert said that I have to use TUSB321 to control CC and FLIP pins of TUSB1044.
so my customer added TUSB321AI to their product, and I want you to ask reviewing this schematic.
(please review the schematic especially focused on the connection of CC pins and Flip pin.)
and here is other questions;
1. EVM said that the pull-up resistor of OUT1, OUT2, ID pins are 200K. (R17, R18, R42). I think this value is too large. care these values right? (usually we use under 10K as pull-up.)

2. should I use inverting buffer between FLIP pin of TUSB1044 and DIR pin of TUSB321AI? or can we use it without inverting?
Please check these issues. Thanks.
Best regards,
Chase