Part Number: TPS65988
Hello TI,
We are using USB pd for the Sourcing power at the levels of 5V-3A , 9V-3A , 15V-3A , 20V - 3A.
But the Device is sourcing the power the at the range of 5V and 900mA.
If Power bank is connected to the PD the Controller is resetting continuously
I have attached my project file please find the attachment and suggest me regarding this issue.
I am getting the Variable voltages triggered by the gpio without load when I connect it to any device they are restarting continuously.