This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: About PDB pin of DS90UB954...

Part Number: DS90UB954-Q1


Dear Sirs,

I have a question about the PDB pin.

In the datasheet, the PDB pin must keep more than 1.5V to enable the IC and there is 50Kohm internal pull-down resistor.

However, as the connection below in the datasheet, if connect to 1.8V with 33Kohm, the PDB will be around 1.08V, right?

(voltage divided with 33K and 50K from 1.8V)

This connection will work or not?

Please help to clarify if there is any misunderstanding about it.

Thanks.