Part Number: DS90UB941AS-Q1
Dear expert,
For dual link mode, is there any requirement for signal latency difference through two cable? For example, one cable is 5m, another cable is 10m. Is it OK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Dear expert,
For dual link mode, is there any requirement for signal latency difference through two cable? For example, one cable is 5m, another cable is 10m. Is it OK?
Hello Ryan,
For dual link mode the two cables should be part of the same assembly and should be the same length. For independent operation where the two FPD ports go to separate deserializers there is no length matching requirement between DOUT0 and DOUT1
Best Regards,
Casey
Casey,
For dual link mode to the same deserializer, what is the max length difference can tolerate?
Thanks
Hello Ryan,
For dual link mode the max pair to pair skew is 1 PCLK cycle. So for example if the pixel clock is 148.5MHz, the max prop delay difference should be ~6.7ns based on the electrical prop delay through the cable.
Best Regards,
Casey