Part Number: SN75LVCP600S
Other Parts Discussed in Thread: DS64BR111
Hi,
I am using SN75LVCP600S SATA redriver . Now I will be doing SI analysis for my board using this driver. My requirement is SATA 3.0. So what should be the value of return loss for RX and TX when measured @3GHz.
The SATA spec says TX Differential return loss @0.3GHz is -14dB. And the Differential slope is mentioned as -13dB. And maximum TX differential loss frequency is mentioned as 3GHz. Now what should be the value of TX differential return loss @3GHz.
Thanks in advance.