Part Number: DS90UB953-Q1
Hi Team,
I am trying to clarify each of the CRC and Parity checks and associated registers when using the 953/954 combo.
I have segmented the CRC/Parity register per data path/type below with some questions. Please correct any identification errors.
BCC:
- 953:
- CRC_ERR_EN (0x1E)
- Enable CRC_ERR alarm
- CRC_ERR (0x52)
- BCC CRC error detected
- CRC_ERR_CLR (0x49)
- BCC CRC Error clear
- RX_PARTIY_CHECKER_ENABLE (953 0x32)
- BCC Parity check enable?
- CRC_ERR_EN (0x1E)
- 954
- BC_CRC _GENERATOR _ENABLE (0x58)
- BCC CRC generator enable
- BCC error detected
- BCC_ALARM (0x51)
- Alarm flag for back channel error from serializer
- IE_BCC_CRC_ERR (0xD8)
- Interrupt on BCC CRC error detect
- BC_CRC _GENERATOR _ENABLE (0x58)
- Questions:
- If there is a CRC error on the BCC, will the 953 stop any I2C transactions from going to its I2C bus?
- The default for the 954 BC_CRC_GENERATOR_ENABLE is enabled.
- Is there any register that needs to be written on the 953 side to enable BCC CRC error checking?
- If you disable the CRC generator, will the 953 automatically recognize there is no CRC and transmit all I2C to its I2C bus from the BCC (permitting that the I2C/alias settings are correct)?
- Is BCC_SEQ_ERROR related to a CRC/Checksum or parity error?
- Is RX_PARITY_CHECKER_ENABLE a parity check for the received BCC frame?
- If so, this is confusing as the 954 has the same named feature/register bit but for the forward channel, and there is no explanation on the 953 datasheet for it.
- I don't see a register setting in the 954 to enable/disable BCC parity bit, is it always on?
Forward Channel:
- 953
- CRC_TX_GEN_ ENABLE (0x02)
- Enable/Disable Forward Channel CRC?
- CRC_TX_GEN_ ENABLE (0x02)
- 954
- RX_PARITY_CHECKER_ENABLE (954 0x02)
- FPD-Link III Parity Checker Enable
- PARITY_ERROR (0x4D)
- FPD-Link III parity errors detected
- FPD3_ENC_CRC_DIS (0xBA)
- Enable/Disable FPD-Link III encoder CRC
- FPD3_ENC_CRC_CAP (0x4A)
- Enable/Disable CRC error flag from FPD-Link III encoder
- RX_PARITY_CHECKER_ENABLE (954 0x02)
- Questions:
- In the 954 datasheet it talks about the RX_PARITY_CHECKER being related to the "received FPD-Link III frame". To me that says the 954 received the frame, and its the forward frame parity. Is the RX_PARITY_CHECKER_ENABLE in the 953 the same parity or is it a separate parity for the BCC?
- Is there a need to enable the forward channel parity on the 953 side?
- Is CRC_TX_GEN_ ENABLE a CRC generated for the full forward channel frame (CSI-2 + control + I2C) by the 953?
- Is the the CRC that the FPD3_ENC_CRC_DIS setting is dealing with?
- In the 954 datasheet it talks about the RX_PARITY_CHECKER being related to the "received FPD-Link III frame". To me that says the 954 received the frame, and its the forward frame parity. Is the RX_PARITY_CHECKER_ENABLE in the 953 the same parity or is it a separate parity for the BCC?
CSI-2:
- 953
- CSI_CHKSUM_ERR_EN (0x1C)
- CSI-2 Checksum Error Alarm Enable
- CSI_ERR_CNT (0x5C)
- CSI-2 Error Counter Register
- CHKSUM_ERR (0x5D)
- Indicates a checksum error detected in the incoming data (uncorrectable).
- CSI_CHKSUM_ERR_EN (0x1C)
- 954
- CSI_CHKSUM_ERR (0x54)
- CSI-2 checksum error from serializer
- CSI_FWD_CKSUM (0x6D)
- Forward CSI packets with checksum errors
- CKSUM_ERR (0x7A)
- Data Checksum Error detected for received CSI packet
- CSI_CHKSUM_ERR (0x54)
- Questions:
- Is the CSI_CHKSUM_ERR_EN considered the enable/disable for the 953 to calculate and check the CSI-2 frame CRC?
BIST:
- 953
- BIST_CRC_ERR
- BIST_CRC_ERR_ CLR
- BIST_BC_ ERRCNT
- CRC_ERR_CNT1/CRC_ERR_CNT2 ?
- CHKSUM_ERR
- 954
DCA:
- 953
- DCA_CRC_EN (0x33)
- DCA CRC Enable
- DCA_CRC_EN (0x33)
- Questions:
- I don't see any mention of a DCA CRC in the 954, is it utilized by the 954?
Thanks,
Justin Bohr