Part Number: TFP410
After reading the datasheet and browsing the E2E forum, I have the following clarification questions about the TFP410.
1. If the hot plug feature isn't used, can the HTPLG pin be left floating?
2. Is Section 7.4.4 stating that the TFP410 must be reset after every powerup or only after momentarily bringing ISEL/RST low and then back high?
3. Also in section 7.4.4 the datasheet states "the device must be reset". Are they referring to using the PD pin, ISEL/RST pin, or the PD bit in CTL_1_MODE register to reset the TFP410?