Part Number: TCAN332G
To protect a TCAN332G CAN transceiver for surge test at the CAN-H and CAN-L lines we need a hint which TVS may be suitable.
The input range is limited to +/-14V. How it is internal protected? If we use a bidirectional TVS for 12V (common mode input range), voltages higher as 20V may occur during 8/20µs Surge test (IEC61000-4-5) with 500V test level. TVS for example is a SP4022-01FTG-C from Littlefuse.
Will the TCAN332G device be damaged?
A split termination will be present. Is a larger capacitance at the split termination to ground helpful to limit the peak voltages during surge test?