Part Number: SN65DP159
Hello Sir:
It's our first time to use SN65DP159.
Would you please help us to check our schematic?
Any recommendations please let us know.
Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DP159
Hello Sir:
It's our first time to use SN65DP159.
Would you please help us to check our schematic?
Any recommendations please let us know.
Thanks a lot.
Hi David:
We have been modified our schematic.
Please help to check again, and we don't understand that mean of "add the DDC snooping option".
Would you please help to explain?
Thanks a lot.
Hi,
The updated schematic looks OK. For DDC snooping option,
The SNx5DP159 uses clock stretching for DDC transactions. As there are sources and sinks that do no perform this function correctly a system may not work correctly as DDC transactions are incorrectly transmitted/received. To overcome this a snoop configuration can be implemented where the SDA/SCL from the source is connected directly to the SDA/SCL sink. The SNx5DP159 will need its SDA_SNK and SCL_SNK pins connected to this link in order to the SNx5DP159 to configure the TMDS_CLOCK_RATIO_STATUS bit. Care must be taken when this configuration is being implemented as the voltage levels for DDC between the source and sink may be different, 3.3 V vs 5 V.
Thanks
David