Part Number: DS90UB927Q-Q1
Other Parts Discussed in Thread: DS90UB940N-Q1,
Hi, TI Support Team
Customers are developing applications using the following products and mass-producing them.
Deserializer: DS90UB940N-Q1
Serializer: DS90UB927Q-Q1
Serializer and deserializer are respectively mounted on different boards, and it is a concept in which two products are connected to receive video signals to complete one product.
During mass production, some products have defects that do not receive video signals properly. In this case, the signal input to the deserializer is checked as low.
1. Is there any problem with the compatibility between the serializer and the deserializer currently being used?
2. The figure below shows the top marking of the normal part (Serializer) and the defective part (Serializer). Is there any difference in the characteristics of serializer chip parts? (I think there should be no difference.)
[Top marking of the normal part (Serializer)]
[Top marking of the defective part (Serializer)]
Please let us know if there is anything necessary to check the bad symptoms.
Thanks.
Regards,
MJ