This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: 1280*640

Part Number: DS90UB941AS-Q1

Dears,
Please help advise on how to configure registers,

PN#: DS90UB941AS-Q1 -> DS90UB928
1280*640@60

Best regard,

Verna

  • Hello Verna,

    See below for an example script - please adjust the TSKIP_CNT as needed based on the DSI clock rate used in your system here. I used 162MHz (54.07MHz PCLK rate) as an example: 1280*640*60*1.1 = 54.07MHz

    # 1280x720p60, Dual Link FPD III
    # PCLK = 54.07MHz
    # DSI clock = 162.2MHz
    # DSI Lane Speed = 324.4Mbps/lane
    # 4 Lanes DSI
    # DSI input port 0
    # DSI non-burst mode with sync pulses 
    # MODE_SEL0 strap = No. 3
    # MODE_SEL1 strap = No. 0 or 1
    
    import time
    
    UB941AS = 0x18
    
    board.WriteI2C(UB941AS,0x01,0x02) # Reset
    time.sleep(0.1)
    board.WriteI2C(UB941AS,0x01,0x08) # Disable DSI
    
    board.WriteI2C(UB941AS,0x40,0x04) # TSKIP_CNT
    board.WriteI2C(UB941AS,0x41,0x05) # TSKIP_CNT
    board.WriteI2C(UB941AS,0x42,0x0C) # TSKIP_CNT
    
    board.WriteI2C(UB941AS,0x40,0x10) # Init DSI Clock Settings (From Section 10.2 of datasheet)
    board.WriteI2C(UB941AS,0x41,0x86) # Init DSI Clock Settings (From Section 10.2 of datasheet)
    board.WriteI2C(UB941AS,0x42,0x0A) # Init DSI Clock Settings (From Section 10.2 of datasheet)
    board.WriteI2C(UB941AS,0x41,0x94) # Init DSI Clock Settings (From Section 10.2 of datasheet)
    board.WriteI2C(UB941AS,0x42,0x0A) # Init DSI Clock Settings (From Section 10.2 of datasheet)
    
    board.WriteI2C(UB941AS,0x01,0x00) #Release DSI

    Best Regards,

    Casey